Technical FAQs

Ask a Question

What is GENIO and GENANAIO modules in Modicon Quantum range.

Go through the description as below:

GENANAIO:  It is a generic analog input/output module

GENIO: It is a generic digital input/output modules.

These module can be used only with partner modules (Spectrum Control , Niobrara,Prosoft etc.). 
All the specific parameters to be entered for correct use of a given module are provided by the company that manufactures this module(personality, number of input/output words, BCD I/O, etc.). 
Was this helpful?
What can we do to improve the information ?