Browse FAQs

Can ATV320 be powered by DC bus using Bonitron unit?

Published date: 14 August 2019

Issue:
Can ATV320 be powered by DC bus using Bonitron unit?

Product Line:
ATV320, Altivar 320

Environment:
All

Cause:
Customer has 1-phase line power.

Resolution:
Technically, if the Bonitron unit is sized properly, it could work. However, We have not tested that combination, and we have no UL listing on it.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.