Technical FAQs

Ask a Question

How to Upgrade the Firmware of M172 through USB

The procedure to load the M172 firmware through USB is as below :-
  • Take an USB key formatted in FAT32
  • Put the Msk596_604_170315.bin file on the USB key
  • Switch off the PLC
  • Put the USB key
  • Switch on the PLC
  • Wait for loading until JACIR menu « HOME »
  • Switch off the PLC
  • Remove the USB key
  • Switch on the PLC

 
Was this helpful?
What can we do to improve the information ?