Technical FAQs

Ask a Question

What are the LED indication on GV4 MPCB.

Front indications
a) Green "Ready" LED: flashes slowly when the circuit breaker is ready to trip in the
event of a fault.
b) Red alarm LED: goes ON when the thermal image of the motor is greater than
95 % of the permissible temperature rise
Was this helpful?
What can we do to improve the information ?