Technical FAQs

Ask a Question

What are the accessories required to upgrade the modicon quantum CPU firmware.

Below are the accessories to upgrade CPU OS:

+ Modbus ( RJ45 port on PLC front panel ) Protocol:

-       USB to Com converter: TSXCUSB232

-       Adaptor RJ45 connector for 140CPU67160: 110XCA20300

-       Modbus port RJ45 for 140CPU67160 3m: 110XCA28202

+ Modbus Plus ( 9-way female SUB-D port on front panel ) Protocol:

-       Modbus plus USB converter: TSXCUSBMBP

-       Modbus plus port 9 way SUB-D for PLC: 990NAD21810
Was this helpful?
What can we do to improve the information ?