Technical FAQs

Ask a Question

What are the shock and vibration resistance values for GV4 MPCB.

For GV4L and GV4LE

Shock Resistance Conforming to IEC 60068-2-27 : 15g - 11 ms

Vibration Resistance Conforming to IEC 60068-2-6: 2.0 to 13.2 Hz and amplitude ±1 mm,13.2 to 100 Hz acceleration 0.7 g.

For GV4P, GV4PE, GV4PEM

Shock Resistance Conforming to IEC 60068-2-27 : 15g - 11 ms

Vibration Resistance Conforming to IEC 60068-2-6: 2.0 to 13.2 Hz and amplitude ±1 mm,13.2 to 100 Hz acceleration 0.7 g.
Was this helpful?
What can we do to improve the information ?