Technical FAQs

Ask a Question

How can we change the Real time clock value of M340 CPU from program or GUI.

Real time clock can be managed remotely by using System word %SW49 to %SW53 which is for Real-time clock function. to write the value from program or GUI, %S50 bit should be set as 1 using unity Pro software.

These words are managed by the system when the bit %S50 is set to 0. 
These words can be written by the user program or by the terminal when the bit %S50 is set to 1. 

Was this helpful?
What can we do to improve the information ?