Technical FAQs

Ask a Question

How to create a hyperlink from a Mimic item to a Map item in clearscada.

To create a hyperlink from a Mimic item to a Map item in the database:

1. In Design Mode, display the Mimic that you want to work with.

2. Either:
• Drag and drop a Map database item from the Database Bar onto the Mimic.
ClearSCADA will then create a text box on the Mimic and automatically create a hyperlink from it to the Map.
To append parameters, or otherwise change the hyperlink URL, you will need to use the Pick Action Wizard to edit the hyperlink URL.
• Use the Pick Action Wizard to create a Hyperlink pick action that has its URL set to the Map database item.
• Use the Animations feature to set the value of PickParam to the address of the Map database item.

3. Save the Mimic.
Was this helpful?
What can we do to improve the information ?