Technical FAQs

Ask a Question

Process to achieve Time sync in PM8240

Time Sync can be performed using option Clock > TimeZone > Cl1 Clock Source.
Clock source have three options which be configured as per the site network/architecture.
Options are:
• Internal: the meter’s internal clock.
• Line frequency: the frequency of the measured power system as the clock source.
• COMM: the meter’s communication port (used by the GPS time sync source).
Was this helpful?
What can we do to improve the information ?