Technical FAQs

Ask a Question

Vamp display is not showing anything & is in blank mode.

The above issue is mostly with respect to the display settings, in most of the cases the display contrast settings are not correct.
The recommended display contrast for all Vamps across all models is 110 for a clear display. Refer attached snapshot.
Was this helpful?
What can we do to improve the information ?