Technical FAQs

Ask a Question

What is the continous current capacity of Control Relay Outputs in Sepam S20.

The contacts O1,O2 & O11 are the control relay outputs in Sepam S20 having the Continous current capacity of 8A
Note: The relay outputs O1,O2,O11 contact comply with clause 6.7 of standard C37.90(30A, 200ms, 2000 operations)
Was this helpful?
What can we do to improve the information ?