Technical FAQs

Ask a Question

Which temperature Sensor is used along with Sepam S20.

Type of sensor used : Pt100 Ni 100/120
Current injected in sensor is 4mA
maximum distance between sensor & Module can be 1Km(0.63mi)
 
Was this helpful?
What can we do to improve the information ?