Technical FAQs

Ask a Question

How to set the number of COMTRADE files to be recorded in PM8240

Depth is the parameter using which we can set the valueThe COMTRADE module’s Depth register determines 
the number of COMTRADE records stored on your meter’s FTP site.
Depth: default value is 1 (the number of COMTRADE records that are storedon the meter’s FTP site.) COMTRADE depth can 
also be configured inLogging > Memory, where the log file memory allocations are listed. An error message will be displayed 
if you enter a value that exceeds the available memory.The maximum for COMTRADE depth is 75, it is fixed
Was this helpful?
What can we do to improve the information ?