Technical FAQs

Ask a Question

What's the function or role of the two MX in Motormechanism.

The ordering code of both Closing & Opening release MX & XF is same.Hence it will show two numbers of "33661"
 Refer trhe snapshot attached.
Was this helpful?
What can we do to improve the information ?