Technical FAQs

Ask a Question

What is the total number of pixels which can be loaded in Vijeo XD 2.4.0 Runtime.

The total number of pixels loaded in runtime can be up to 10,000,000 pixels. If this exceeds, then somes images might not
be visible. The pixel for an image can be checked by its properties (Right click image > Properties > Details).

Option is that you can reduce the external image pixel by opening it in paint. Right click image > open with paint > Click Resize and reduce the pixels. After that re-import it in VXD.
Was this helpful?
What can we do to improve the information ?