Technical FAQs

Ask a Question

Is there any method to change the the encoder usage between "machine" and "none" without restart of the drive ?

Yes, It is possible to change ENC_ModeoFMaEnc (Modbus address 20484) in state RDY to none without reboot of the drive and then actual position is taken from encoder 1.
Was this helpful?
What can we do to improve the information ?