Technical FAQs

Ask a Question

What are the models of AS-Bs with different I/O point count and I/O mix.

AS-B comes in eight models with different I/O point count and I/O mix. Below are the details.
 
Model I/O Points
AS-B-24 24
AS-B-24H 24
AS-B-24L 24
AS-B-24HL 24
AS-B-36 36
AS-B-36H 36
AS-B-36L 36
AS-B-36HL 36
Was this helpful?
What can we do to improve the information ?