Technical FAQs

Ask a Question

Do Micom P24x relays conforms to Shock & Bump tests.

The Micom P24x relays conforms to Shock & Bump tests as per EN / IEC 60255-21-2: 

Shock response Class 2
Shock withstand Class 1
Bump Class 1
Was this helpful?
What can we do to improve the information ?