Technical FAQs

Ask a Question

Do MiCOM P24x relays conforms to Vibration tests.

The MiCOM P24x relays conforms to Vibration tests as per EN / IEC 60255-21-1 :
Response Class 2
Endurance Class 2
Was this helpful?
What can we do to improve the information ?