Technical FAQs

Ask a Question

Do MiCOM P24x relays conforms to Conducted emission tests.

The MiCOM P24x relays conforms to Conducted emission tests as per CISPR 22 Class A:
Power supply:
0.15 - 0.5 MHz, 79 dBμV (quasi peak) 66 dBμV (average)
0.5 - 30 MHz, 73 dBμV (quasi peak) 60 dBμV (average)
Permanently connected communications ports:
0.15 - 0.5MHz, 97dBμV (quasi peak) 84dBμV (average)
0.5 - 30MHz, 87dBμV (quasi peak) 74dBμV (average)
Was this helpful?
What can we do to improve the information ?