Technical FAQs

Ask a Question

Why parameter tq0 is not visible on ATS48 Soft Starter.

 
tq0 is used to program Initial starting torque and it is not present visible in CLP=OFF because we have not torque control.  In CLP=off, the torque is not managed but only the voltage and current. Note: tq0 is visible when CLP=ON.

 
Was this helpful?
What can we do to improve the information ?