Technical FAQs

Ask a Question

Do MiCOM P24x relays conforms to Power Frequency Magnetic Field Immunity tests.

The MiCOM P24x relays conforms to Power Frequency Magnetic Field Immunity tests as per EN / IEC 61000-4-8, Level 5,
100 A/m applied continuously, 1000 A/m applied for 3 s.
-> As for EN / IEC 61000-4-9, Level 5,
1000 A/m applied in all planes.
-> As for EN / IEC 61000-4-10, Level 5,
100 A/m applied in all planes at 100 kHz and 1 MHz with a burst duration of 2 s.
Was this helpful?
What can we do to improve the information ?