Technical FAQs

Ask a Question

Do MiCOM P24x relays conforms to Radiated Immunity from Digital Communications.

The MiCOM P24x relays conforms to Radiated Immunity from Digital Communications as per CISPR 22 Class A:
30 to 230 MHz, 40 dBμV/m at 10m measurement distance
230 to 1 GHz, 47 dBμV/m at 10 m measurement distance.
1 – 3GHz, 76dBμV/m (peak), 56dBμV/m (average) at 3m measurement distance.
3 – 5GHz, 80dBμV/m (peak), 60dBμV/m (average) at 3m measurement distance.
Was this helpful?
What can we do to improve the information ?