Technical FAQs

Ask a Question

Do MiCOM P24x relays conforms to Radiated Immunity from Digital Radio Telephones.

The MiCOM P24x relays conforms to Radiated Immunity from Digital Radio Telephones as per EN / IEC 61000-4-3: 10 V/m, 900 MHz and 1.89 GHz.
Was this helpful?
What can we do to improve the information ?