Technical FAQs

Ask a Question

Do MiCOM P24x relays conforms to Surge Immunity tests.

The MiCOM P24x relays conforms to Surge Immunity tests as per EN / IEC 61000-4-3: 10 V/m, 900 MHz and 1.89 GHz.EN / IEC 61000-4-5, EN / IEC 60255-26:
Time to half-value: 1.2 to 50 μs,
Amplitude: 4 kV between all groups and case earth (ground),
Amplitude: 2 kV between terminals of each group.
Amplitude: 1kV for LAN ports
Was this helpful?
What can we do to improve the information ?