Technical FAQs

Ask a Question

Do MiCOM P24x relays conforms to 1 MHz Burst High Frequency Disturbance Test.

The MiCOM P24x relays conforms to 1 MHz Burst High Frequency Disturbance Test as per EN / IEC 60255-22-1, Class III,
Common-mode test voltage: 2.5 kV,
Differential test voltage: 1.0 kV,
Test duration: 2 s,
Source impedance: 200 ohms
(EIA(RS)-232 ports excepted).
Was this helpful?
What can we do to improve the information ?