Technical FAQs

Ask a Question

UL Listed MCCB above 630A

The Compact NS630b-1600 range MCCBs are not UL listed.

If you need UL listed MCCB >630A circuit breakers, you have to opt-to the Power pact M-frame, P-frame and R-frame ranges by Schneider Electric (Square D)

Please refer the link provided below to download the catalogue for the same:

https://www.schneider-electric.us/en/product-range-download/1853-powerpact-m-frame-molded-case-circuit-breakers#tabs-top

 
Was this helpful?
What can we do to improve the information ?