Technical FAQs

Ask a Question

Is early-make or early-break contacts are available in INF*32 to INF*800

Yes this facility is available in INF*32 to INF*800

CAM (early-make or early-break function): indicates the position of the
switch-disconnector fuse handle.

Used in particular for:
CAO early-break contact (auxiliary contacts open before the main contacts), used
for example to automatically open a circuit breaker or a contactor before opening the
switch-disconnector fuse

CAF early-make contact (auxiliary contacts closed before the main contacts)
Was this helpful?
What can we do to improve the information ?