Technical FAQs

Ask a Question

Which contacts blocks are supplied with XALD101H29 Push button station?

The XALD101H29 is supplied with ZENL1111 NO Contact.
The reference for NC Contact is ZENL1121.
Was this helpful?
What can we do to improve the information ?