Technical FAQs

Ask a Question

Difference between Blown-fuse indicator and Fuse monitor for Fupact INF

Fuse Monitor device is used to remotely indicate the status of standard fuses (without strikers) whereas Blown-fuse indicator is used to remotely indicate the status of fused with strikers (NFC or DIN).

Although both provide same function :- 
Signaling a blown fuse
Protecting motors from overloads caused by single-phase operation
Preventing the risks of abnormal voltages on the neutral.
Was this helpful?
What can we do to improve the information ?