Technical FAQs

Ask a Question

Can the digital outputs be reprogrammed.What are the ET 1 and ET 2 settings.

The digital outputs can each be configured to pulse for one of the following:
(k)Wh Del., (k)VAh, (k)VARh Del., (k)Wh Rec., (k)VARh Rec.
In Ext 1 and Ext 2 mode, the digital output state is determined by a Modbus register value (1 for ON and 0 for OFF).
Was this helpful?
What can we do to improve the information ?