Technical FAQs

Ask a Question

What is the Inductance (µH) and Current (Amp) rating for ATV61 Drive output choke ?

Below are the Inductance (µH) and Current (Amp) rating for ATV61 Drive output choke :-

VW3 A5 101 350µH 12A
VW3 A5 102 120µH 48A
VW3 A5 103 80µH 90A
VW3 A5 104 50µH 215A
VW3 A5 105 40µH 314A
VW3 A5 106 25µH 481A
VW3 A5 107 15µH 759A
VW3 A5108 10µH 1188A

 
Was this helpful?
What can we do to improve the information ?