Technical FAQs

Ask a Question

What is the maximum torque rating for the ATV900 drive ?

In ATV900 Maximum torque  can be supplied up  to 180% of Tn (Nominal Torque) on any type of motor in open or closed loop control.
Was this helpful?
What can we do to improve the information ?