Technical FAQs

Ask a Question

Can we provide the DC input for ABL8REM24050 power supply ?

The ABL8REM24050 can be supplied by 110 or 220 VDC.
It is technically possible to use DC voltage input as well as AC voltage input with ABL8REM24050 Power supply. .
- There is no separate connection diagram for 110 or 220 Vdc, you can connect to L (dc +) & N(dc -).

Was this helpful?
What can we do to improve the information ?