Technical FAQs

Ask a Question

Is Line load reversible possibility in xID type RCCB?

Yes, line load reversibility is available in xID type RCCB. Incoming supply cables can be connected to either the top or bottom terminals as required.
Was this helpful?
What can we do to improve the information ?