Technical FAQs

Ask a Question

What is the recommended cable size for G sense signal wiring for EM6436 and EM6438 dual source meter ?

The cable size recommendation for G sense wiring Connector for EM6436 and EM6438 dual source meter is :- 

For Single Wire: The maximum permissible cross-section is 2.5 sq.mm.
For Two Wires: The maximum permissible cross-section is 1.5 sq. mm.

Kindly refer attached reference document.
Was this helpful?
What can we do to improve the information ?