Technical FAQs

Ask a Question

What is the temperature characteristic of Powertag.

The temperature characteristic of Powertag is as follows:

Operating temperature >>> -25°C to 60°C
Storage temperature    >>> -40°C to 85°C
Was this helpful?
What can we do to improve the information ?