Technical FAQs

Ask a Question

What is compatible circuit breaker which can be used with PowerTag.

Below are the details of compatible circuit breaker and switches with PowerTag.

«Single terminal» circuit breakers and switches at intervals of 18 mm, ratings
less than or equal to 63 A:
• Acti 9 : iC60/iID/iID K/iSW (< 63 A)/iSW-NA/Reflex iC60/iK60/i65N-K
• Multi9 : C32/C45/C60/K60/ID/ISW/I-NA
• DT60
Was this helpful?
What can we do to improve the information ?