Technical FAQs

Ask a Question

What is the Creepage Distances and Clearances of Easergy Micom P132 protection relay.

The Creepage Distances and Clearances of Easergy Micom P132 protection relay are
● Per EN 60255-27 standard.
● Pollution degree 3, working voltage 250 V,
● overvoltage category III, impulse test voltage 5 kV.
Was this helpful?
What can we do to improve the information ?