Technical FAQs

Ask a Question

Do MiCOM P132 relays conforms to 1 MHz Burst Disturbance Test.

The MiCOM P132 relays conforms to 1 MHz Burst Disturbance Test as per EN 60255-22-1, Class III.
● Common-mode test voltage: 2.5 kV.
● Differential test voltage: 1.0 kV.
● Test duration: > 2 s.
● Source impedance: 200 Ω.
Was this helpful?
What can we do to improve the information ?