Technical FAQs

Ask a Question

Do MiCOM P132 relays conforms to Immunity to Electrostatic Discharge Test.

The MiCOM P132 relays conforms to Immunity to Electrostatic Discharge Test as per EN 60255-22-2 and IEC 60255-22-2, severity level 4.
Contact discharge
● Single discharges: > 10.
● Holding time: > 5 s.
● Test voltage: 8 kV.
● Test generator: 50 to 100 MΩ, 150 pF / 330 Ω.
Was this helpful?
What can we do to improve the information ?