Technical FAQs

Ask a Question

Do MiCOM P132 relays conforms to Immunity to Radiated Electromagnetic Energy Test.

The MiCOM P132 relays conforms to Immunity to Radiated Electromagnetic Energy Test as per EN 61000‑4‑3 and ENV 50204, severity level 3.
● Antenna distance to tested device: > 1 m on all sides.
● Test field strength, frequency band 80 to 1000 MHz: 10 V / m.
● Test using AM: 1 kHz / 80 %.
● Single test at 900 MHz: AM 200 Hz / 100%.
Was this helpful?
What can we do to improve the information ?