Technical FAQs

Ask a Question

Do MiCOM P132 relays conforms to Electrical Fast Transient or Burst Requirements Test.

The MiCOM P132 relays conforms to Electrical Fast Transient or Burst Requirements Test as per EN 61000-4‑4 and IEC 60255‑22‑4, severity levels 3 and 4.
● Rise time of one pulse: 5 ns.
● Impulse duration (50% value): 50 ns.
● Amplitude: 2 kV / 1 kV or 4 kV / 2 kV.
● Burst duration:15 ms.
● Burst period: 300 ms.
● Burst frequency: 5 kHz.
● Source impedance: 50 Ω.
Was this helpful?
What can we do to improve the information ?