Technical FAQs

Ask a Question

Do MiCOM P132 relays conforms to Power Frequency Immunity Test.

The MiCOM P132 relays conforms to Power Frequency Immunity Test as per IEC 60255‑22‑7, Class A:

Phase-to-phase
● RMS value 150 V.
● Coupling resistance 100 Ω.
● Coupling capacitor 0.1 μF, for 10 s.
Phase-to-ground
● RMS value 300 V.
● Coupling resistance 220 Ω.
● Coupling capacitor 0.47 μF, for 10 s.
To comply with this standard, it is suggested to set the parameter (010 220)
INP: Filter to 6 [steps].
Was this helpful?
What can we do to improve the information ?