Technical FAQs

Ask a Question

Do MiCOM P132 relays conforms to Immunity to Conducted Disturbances Induced by Radio Frequency Fields Test.

The MiCOM P132 relays conforms to Immunity to Conducted Disturbances Induced by Radio Frequency Fields Test as per EN 61000-4-6 and EN 60255-22‑6, severity level 3.
● Test voltage: 10 V.
Was this helpful?
What can we do to improve the information ?