Technical FAQs

Ask a Question

Do MiCOM P132 relays conforms to Power Frequency Magnetic Field Immunity Test.

The MiCOM P132 relays conforms to Power Frequency Magnetic Field Immunity Test as per EN 61000-4-8 or IEC 61000-4-8, severity level 4.
● Test frequency: 50 Hz
● Test field strength: 30 A / m.
Was this helpful?
What can we do to improve the information ?