Technical FAQs

Ask a Question

How we can operate varlogic APFC relay RT-series in manual mode ?

When RT is in Manual Mode, capacitor steps are  connected by pressing UP button.
Each time UP button is pressed, C+ light is ON and one step is connected after set response
delay time.
NORMAL light will be ON after the connection of the step. This operation must be repeated
to  connect more steps.
Capacitor steps  are  disconnected by pressing DOWN button. Each time DOWN button is
pressed, C- light is ON and one step is disconnected after set response delay time. NORMAL
light will be ON after the disconnection of the step. This operation must be repeated to
disconnect more steps.
 
Was this helpful?
What can we do to improve the information ?