Technical FAQs

Ask a Question

Can we use communicating type MN and XF for source changeover system.

MX/XF communicating releases are of the impulse type only and cannot be used to lock a circuit breaker in OFF position.It is
advised to use standard MX or XF releases for applications such as source-changeover systems.
Was this helpful?
What can we do to improve the information ?