Technical FAQs

Ask a Question

What is available in local control interface of LTMCU.

The Local Control Interface consists of 5 control keys and 4 LEDs. The control keys, if active, enable you to control the LTMR. Pressing a control key sends a signal to the LTMR to activate the associated function
Was this helpful?
What can we do to improve the information ?