Technical FAQs

Ask a Question

What is function of control key 1 to 3 of LTMCU when operating mode is independent in LTMR.

Control key performs below defined function in independent operating mode.
Operating mode Assignment Key 1 Key 2 Key 3
Independent 2-wire (maintained) Control motor (O.1) Control O.2 Stopmotor(open O.1) and open O.2 while pressed
3-wire (impulse) Start motor (close O.1) Close O.2 Stop motor(open O.1) and open O.2
Was this helpful?
What can we do to improve the information ?